Other Parts Discussed in Thread: LMP91000
I have a chemical gas sensor and I need to build an electronic interface for it. I have the LMP91000 eval board. At one time I thought I'd need a simple potentiostat, which the LMP91000 would work well for. However, as I have progressed I've found the best way to operate the sensor is as a resistive device whose resistance changes with exposure to the gas. I've been using a precision digital multimeter to do 4 wire ohmic measurements thus far. Basically the DMM puts a fixed current through the sensor and monitors its voltage to determine overall resistance. Can the LMP91000 be set up to output a constant current (like 0.1 or 1mA) and measure the resulting voltage?