Part Number: DP83TC814R-Q1
Tool/software:
Could you please review the circuit for RMII slave mode configuration ad provide input


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC814R-Q1
Tool/software:
Could you please review the circuit for RMII slave mode configuration ad provide input


Hi Nayan,
I am reviewing the schematic and will have feedback shortly.
Best,
Evan Su
Hi Nayan,
The schematic generally looks good. I have just a few notes:

Best,
Evan Su
Hi Nayan,
ok I will look into the comments shared, Could you please share the isolated connectors that can be connected to TRD_M & TRD_P lines?
The isolation I mentioned isn't really related to TRD_M and TRD_P or a special type of connector. My meaning was that in a case where the cable is shielded, typically the ground used by the connector + shield and the ground used by the PCB are different nets, and then these nets can be connected or disconnected through the isolation capacitor and isolation resistor placeholders as needed. The MDI termination network would typically be referenced to the connector/shield ground instead of the PCB ground in this case. If you are not using a shielded cable then typically this does not matter, it's common for there to only be one ground in the design then.
I have one more query , In RMII slave mode the 50MHz oscillator used should it be external or is it coming from uC (because MCU STM32 is host in our application)?
I haven't personally tried that, but the 50 MHz oscillator input could come from any source that meets the clock specifications in section 7.6 of the datasheet.
Best,
Evan Su