This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL16C754C: Interface forum

Part Number: TL16C754C

Tool/software:

UART-ICのデータシートについて質問があります:TL16CP754C。 TL16CP754Cデータシートのトップページに「3.3V動作用の32MHz発振器入力クロック(2Mbps)」と記載されています。 これは、動作電圧3.3Vで使用すると、32MHzの発振器入力で最大2Mbpsの通信速度が使用できるということですか? 現在、私は3.3V電源でICを実行しており、24.576MHzの発振器出力はXTAL1ピンに接続されています。 このICは使用できますか?

Sorry. The previous question may have been forwarded in Japanese, so I will resend it in English.

I have a question about the datasheet for the UART-IC: TL16CP754C. On the top page of the TL16CP754C datasheet, there is a statement that says, "32-MHz Oscillator Input Clock (2 Mbps) for 3.3-V Operation." Does this mean that when used with an operating voltage of 3.3V, a 32 MHz oscillator input can be used for communication rates of up to 2 Mbps? Currently, I am running the IC on a 3.3V power supply, and the 24.576 MHz oscillator output is connected to the XTAL1 pin. Is this acceptable for using this IC?