This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD3S716-Q1: Schematic review

Part Number: TPD3S716-Q1

Tool/software:

Hi Teams,

Please help to review schematic for TPD3S716-Q1, thanks.

  • Hello Che Wen,

    Please see feedback below:

    • The recommended VBUS_CON cap is 1uF rated for 100V
    • The recommended VBUS_SYS cap is 100uF rated for 10V
    • The recommended VIN cap is 10uF rated for >6.3V
    • It is recommended to switch the placement of the CMC and inductors as shown in the diagram below.

    BR,

    Seong