Part Number: SN65C3221E
Tool/software:

In the above image I have marked two boxes, Basically VOH and VOL values. Kindly provide Minimum and Maximum of VOH, VOL values for DIN Input Pin.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65C3221E
Tool/software:

In the above image I have marked two boxes, Basically VOH and VOL values. Kindly provide Minimum and Maximum of VOH, VOL values for DIN Input Pin.
Hi Karthik,
The VIH range is from 2V to 6V, and the VIL range is from -0.3V to 0.8V. The max VIH and min VIL are just the absolute maximum values mentioned in the previous section of the datasheet.
Let me know if that helps or if you have any other questions!
-Ethan