Part Number: DS160PR810
Other Parts Discussed in Thread: DS100BR410
Tool/software:
I want to perform transmission and reception on a 9.2Gbps SLVS-EC (almost PCIe 4.0).
The differential output voltage of the Tx device is 160 mVpp, while the specification for the differential input voltage of the Rx device is "400 mV or higher."
Since the Rx device is a general-purpose differential signal receiver and does not comply with the SLVS standard,
there is a mismatch between the Tx and Rx differential swing voltages.
I want to resolve this mismatch by inserting a DS160PR810 between the Tx and Rx to achieve an 8dB gain—from 160 mV to 400 mV.
I would like to know if the gain is sufficient. According to the datasheet,
the flat gain is up to 2dB and the EQ (CTLE) is up to 18dB @8GHz,
so can it be interpreted that the differential voltage swing (eye height) can be boosted by 20dB?
If this interpretation is incorrect, please let me know the maximum gain that can be achieved with the DS160PR810.
Additionally, the datasheet does not specify the input differential voltage range; can this IC receive signals within the range of 160 mV to 280 mV?