This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3232E: Selecting External capacitor (voltage rating and Values)

Part Number: TRS3232E

Tool/software:

Hi,

I have question about selecting External capacitor (C1 to C4) to use with TRS3232EIDR for Vcc = 5V.

from datasheet,

C1–C4 = 0.1 μF at VCC = 3.3 V ± 0.3 V

C1 = 0.047 μF, C2–C4 = 0.33 μF at VCC = 5 V ± 0.5 V.

Questions are

1. How many minimum voltage rating for external cap.? is it depend on Vcc (cap. voltage > Vcc+our margin)?

I notice that design ref. use to 25V. (maximum Vcc of TRS3232E is 6V.) why they not select cap. voltage 10V or 16V?

2. What happen, incase we use C1 to C4 = 0.1uF with Vcc 5V?

Thank you.