Part Number: TCAN1051HG
Other Parts Discussed in Thread: ISO1044
Tool/software:
Hello Team,
We are using the CAN Transceiver TCAN1051HGVDR in one of our products.
These signals from this transceiver is then fed to another transceiver (TCAN1051HGVDR) at the DUT end through SSR (TLP3147(F).
We are using the SSR to MUX the MCU with different DUTs.
Only one pair of SSR will be selected at a time so that only one communication is live between CAN transceivers.
Also, only one DUT will be powered at a time.
Since the SSR has some off state capacitance, the signals will be present at the output of the SSR even when it is off but the device cannot read it because it is powered off and since the signals are not DC biased.
We have termination resistors at all the transceiver sides.
If DUT 2 and 3 are not connected, we have proper communication between MCU and the DUT1.
If DUT2 is connected without termination resistor, then also we have communication between MCU and DUT1 or DUT2.(DUT1 has termination resistor)
If DUT2 is connected with termination resistor, then we are not able to communicate with DUT1 or DUT2.
If DUT3 is connected with the termination resistors, then we are not able to communicate with DUT1 or DUT2 or DUT3
1). What could be the reason for this?
2). Will CAN work with only 1 termination resistor at one end.
3). During off time, no DC current will flow through the SSR, since CAN has pulsating signals, and since AC can pass through the off state capacitance of the SSR, will this load the CAN transmitter?.
4).
Looking for your reply