Part Number: TCAN1465-Q1
Tool/software:
Hi team,
I received questions from my customer regarding CANINT and device behavior.
Could you support below questions?
Q1) Customer asks if CANINT would be set by (a) to (c) cases.
Are below statements for each cases correct?
(a) When device is in Standby mode(SW_EN=0), CANINT can be set If device receives WUP
(b) When device is in Normal mode(SW_EN=0), CANINT can is set if device receives WUP
(c) When device is in Sleep mode(SW_EN=1), CABUBT can be set if device receives WUF.
Q2) Assuming CANINT being set due to the causes shown in above (a) to (c).
After MCU clearing by writing CANINT=1b, is there any chance that CANINT=1b being set again?
In other word, Is it correct understanding that CANINT would be set if device detects WUP or WUF even after MCU clear CANINT?
Q3)
Step1: Device sets CANINT in normal mode due to possible cause
Step2: Device shifts to Sleep mode from Normal mode without clearing CANINT
After step2, will device automatically shift to Standby mode without receiving WUP/WUF?
Best regards,