Part Number: DP83TC814S-Q1
Tool/software:
Hi TI team,
We want to test the INT_N action.
Could you tell us how to trigger below INT action? And how to recovery?
| Bit | Field | Description | How to trigger | How to recovery | |||||
| MISR1 Register (Address = 12h) | 14 | energy_det_int | This INT can be asserted upon Rising edge only of energy_det signal using reg0x101 bit [0] : cfg_energy_det_int_le_only. status output of energy_det_hist signal on reg0x19 bit[10]. 0b = No Change of energy detected 1b = Change of energy_detected (both rising and falling edges) |
||||||
| 13 | link_int | Link status change interrupt 0b = No change of link status interrupt pending. 1b = Change of link status interrupt is pending and is cleared by the current read. |
|||||||
| 12 | wol_int | Interrupt bit indicating that WOL packet is received 0b = No WoL interrupt pending. 1b = WoL packet received interrupt is pending and is cleared by the current read. |
|||||||
| 11 | esd_int | 1 = ESD detected interrupt is pending and is cleared by the current read. 0 = No ESD interrupt pending. |
|||||||
| 10 | ms_train_done_int | 1 = M/S Link Training Completed interrupt is pending and is cleared by the current read. 0 = No M/S Link Training Completed interrupt pending. |
|||||||
| 9 | fhf_int | 1 = False carrier counter half-full interrupt is pending and is cleared by the current read. 0 = No false carrier counter half-full interrupt pending. |
|||||||
| 8 | rhf_int | 1 = Receive error counter half-full interrupt is pending and is cleared by the current read. 0 = No receive error carrier counter half-full interrupt pending. |
|||||||
| MISR2 Register (Address = 13h) | 15 | under_volt_int | 0b = Under Voltage has not been detected 1b = Under Voltage has been detected |
||||||
| 14 | over_volt_int | 0b = Over Voltage has not been detected 1b = Over Voltage has been detected |
|||||||
| 10 | sleep_int | 0b = Sleep mode has not changed 1b = Sleep mode has changed |
|||||||
| 9 | pol_int | 0b = Data polarity has not changed 1b = Data polarity has changed |
|||||||
| 8 | jabber_int | 0b = Jabber not detected 1b = Jabber detected |
|||||||
Best Regards!
Wang Jingkun