Part Number: SN75DP130
Tool/software:
Dear Technical Support Team,
I'd like to lane swap.
For example,
Connect the source side LANE3± to the IN0± pins of the SN75DP130, and connect the OUT0± to the LANE3± on the sink side (DP connector).
According to previous post, It seems to be ok, however should user set some register enable or disable for this comment "you must manually enable all the lanes for the device rather than having the DP130 detect which lanes to turn on."?
If so, could you tell me the steps and what register should change manually for lane swap?
SN75DP130: SN75DP130 DP Lane swap - Interface forum - Interface - TI E2E support forums
If this implementation guide has normal steps, I'd like to know what register should I change .
Implementation Guide: DP130 in a Sink
Regards,
ttd