Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS1204: TMDS1204RNQR

Part Number: TMDS1204
Other Parts Discussed in Thread: TMDS181

Tool/software:

I am planning to use TMDS1204RNQR this IC, in my project. And I need to confirm, whether this IC will support 8K 60 FPs or 120 FPs refresh rate, and in datasheet it is mentioned like this IC will support 12 Gbps speed, and it will work as redriver mode also, and both sink (Rx) and source (Tx) application can use this IC. Please confirm, if I can use this Same part as Sink mode means HDMI IN (Rx) redriver IC and same as Source mode HDMI OUT (Tx) applications. It will support both mode., and please suggest any HDMI 2.1 redriver IC with TMDS181RGZT this package and Pin compatible.

  • Hi Vaishnavi, 

    TMDS1204 can be used as both in sink mode and source mode and can support 8K 120 FPS. 
    Unfortunately, we do not have pin to pin compatible IC to TMDS181 for HDMI 2.1 redriver. 

    Please let me know if you have any other questions. 

    Best,
    J