Part Number: TCAN334G
Other Parts Discussed in Thread: TCAN1462-Q1
Tool/software:
Hello,
CAN communication requirements:
1. The length of single packet communication data on the CAN bus reaches 64 bytes.
2. The CAN communication rate is 20kbps (adjustable depending on the number of nodes).
3. The maximum number of nodes on the bus can reach 400, but at least 200 are required.
4. CAN transceiver explicit timeout, single transceiver failure cannot disrupt bus communication.
The customer has the following questions:
1. Is CAN FD suitable for our usage scenario?
2. Are there any possible hidden dangers? For example, signal interference?
3. The necessity of CAN SIC?
4. Based on the working voltage, power consumption, and other parameters of the integrated chip, it is believed that TCAN334GDR is the most suitable for the requirements.
5. Is TCAN334GDR compatible with the functionality of TCAN334DR, meaning that the current standard CAN can use TCAN334GDR instead of TCAN334DR?
6. What is the difference in operating current parameters between TCAN334GDR and TCAN334DR, especially in the receiving mode?
7. Do you have any other design suggestions?
Thanks!