Part Number: TCAN1465-Q1
Tool/software:
Hi team,
I'm currently working with the TCAN1465-Q1 and have some questions regarding the Fail-safe mode behavior and configuration:
1. Mode transitions after entering Fail-safe Mode
According to Figure 8-10 (state diagram) in the datasheet, it appears that the device may transition from Fail-safe Mode to other modes such as Standby, Sleep, or Any State.
1-1. Are the conditions for these transitions documented somewhere?
I couldn't find clear explanations in the FSM Note, so I would appreciate clarification on:
* What conditions trigger transitions from Fail-safe Mode to other modes?
* if such a transition occurs, will the FSM bit in the INT_3 register be automatically cleared?
(the datasheet mentions that this bit can only be cleared while in Fail-safe mode, so I'd like to understand whether this is done automatically during a transition.)
1-2. when the device remains in Fail-safe Mode, Is SPI communication still available?
The datasheet states that SPI status is determined by the type of fault, but could you clarify:
* Which specific faults affect SPI communication?
* How exactly the SPI behaves under such conditions?
2. Disabling Fail-safe Mode after a fault during startup
Is it possible to disabled the Fail-safe Mode While the device is already in Fail-Safe mode, due to faults that occurred during Startup?
3. Preventing entry into Fail-safe Mode at startup
Is there any way to disable or prevent automatic entry into Fail-safe mode during startup?
Thank you in advance, and I look forward to your reply.
Best regards,