Part Number: TCAN11623-Q1
Tool/software:
Hello,
I'm using a TCAN11623DMTRQ1 (CAN transceiver + LDO 3.3V) with a 10uF connected on VLD03 pin GCJ31CR71C106KA15L
A 10uF with same reference is connected on VFLT
Input capacitors are 220 + 100nF with a 10R in series with Vbat (12V)
I can see a ripple of 76mV (regular ripple is more like 45mW but I can see asynchonous peaks
As a consequence I can see some oscillations on the ADC output captured by the TI microcontroler powered by this LDO
Average consumption of the PCB is around 60mA/12V, on 3.3V side there is a load of around 45mA that is switched on 60ms every 100ms
Would it be possible to know if the chosen capacitor is too low or if a parameter is wrong, please?
Thanks
BR. T.