Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS100BR410: POR Time before operation

Part Number: DS100BR410

Tool/software:

Good day. In SNLS326B (April 2013 revision) the following specification is given for the Serial Management Bus Interface:

tPOR (Time in which a device must be operational after power-on reset) = 500ms (max). 

I would like some clarification on this specification. Does it specify:

a) that the DS100BR410 will be ready to use 500ms (max) after the reset OR

b) that the DS100BR410 has to be configured for operation within 500ms (max) after the reset.

Thank you very much.