Other Parts Discussed in Thread: DS560DF810,
Tool/software:
Hi team,
My customer tested the EVM and found some issues here. can not build up the bench. The new project is significant for us. pls kindly support
I am currently using EVM to follow the steps in the datasheet (DS560DF810 EVM User's Guide) to wire the circuit, and when I execute usefulFunction.py in latte, the following error occurs:
------------------------
#======
#Executing .. selection
------------READBACK CHANNEL INIT STATUS----QUAD : 0-----CH : 0-----
//Command=self.regs.REGGROUP_14.Property_3ch_31_0=0x1
//Triggering Macro - Opcode : 0xc6 Name : READBACK_CH_INIT_STATUS
CHANNEL_INIT_STATUS : 2
HEART_BEAT : 0
CONFIGURATION_SELECTED : 0
Waiting for signal detection. If wait_for_signal_enable feature is used, this state implies device is waiting for signal swing to cross the expected threshold.
Channel initialization is in progress / lock not achieved.
#Done executing .. selection