Part Number: TCAN4550
Tool/software:
Hey ,
We use in our design the TCAN4550 and supply it with 2 different power sources for Vsup(12V) and VIO(3.3V)

We have in our design the possibility to turn off the 3V3DC_P via switch with Fet as below

We found that when we turn OFF the VIO only (Vsup is still 12V) , we still see a voltage on the 3V3DC_P (~1V)
Only after disconnecting the TCAN4550 , VIO become 0 as we expected.
This voltage can come from the Data signals (are PU to 3V3DC_P) or via the VIO.
1. Do you have an idea why its happening ?
2. It is ok to turn OFF the VIO when Vsup is still 12V ?