Part Number: TUSB5461-Q1
Other Parts Discussed in Thread: TUSB1146, TUSB1044A
Tool/software:
We are wanting to design a test board for automotive USB hubs using an active redriver/mux that can be used in two different setups. The first would be used as a PD sink and USB 2/3 5Gbps-device, for this setup we are currently using a TUSB1042 successfully. The new design needs to also be able to switch to being a PD sink and a display port source. What is the best chip to use, TUSB5461, TUSB1146, and TUSB1044A all look promising but we're not sure how to decide. We will include a PD controller/micro combination that can control the mux over I2C and is also capable of negotiating the DP PD routines and DR swap. Thanks.
-Eli Brantingham