Part Number: TMDS181
Tool/software:
Dear Team,
Please find the attached pdf of the TMDS181RGZT and SN65DP159RSBT, please check whether the connections are proper.
Thanks,
Irfan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDS181
Tool/software:
Dear Team,
Please find the attached pdf of the TMDS181RGZT and SN65DP159RSBT, please check whether the connections are proper.
Thanks,
Irfan
Irfan
Please see attached for my review comment and let me know if you have any questions.
Ti HDMI retimer PRJCL-02_TI_Reviewed_06102025.pdf
Thanks
David
Hi David,
1)The EQ_SEL/A0 and A1 is for I2C address select so we have configured it through pull up and pull down, so whether if we leave it floating will there not be any problem? mentioned in 8.5.1 in datasheet
2) The SCL SINK and SDA SINK signals we have connected is 3.3 for TMDS181 will that be fine? can you confirm this once
3) And the SCL SINK and SDA SINK for SN65DP we have connected 5V should this both be same or if varied will there be any issues causing ? can i connect 3.3V to this pin also ?
Thanks,
Irfan
Irfan
1)The EQ_SEL/A0 and A1 is for I2C address select so we have configured it through pull up and pull down, so whether if we leave it floating will there not be any problem? mentioned in 8.5.1 in datasheet
The I2C_EN is pulled low in the schematic so the pin strap mode is being enabled. So my review comment for EQ_SEL/A0 and A1 is geared toward the pin strap mode configuration. In I2C mode, yes, you do need to pull them either high or low to set the I2C address.
2) The SCL SINK and SDA SINK signals we have connected is 3.3 for TMDS181 will that be fine? can you confirm this once
I don't see this as an issue since TMDS181 SCL_SNK and SDA_SNK VI-DC is from -0.3V to 5.5V.

I assume you have a level shifter that shifts from 3.3V to 5V, and also have 47k pullup on the DDC for the HDMI input design?
3) And the SCL SINK and SDA SINK for SN65DP we have connected 5V should this both be same or if varied will there be any issues causing ? can i connect 3.3V to this pin also ?
DP159 SDA_SNK and SCL_SNK need to be connected to 5V.
Thanks
David
Hi David,
Thanks for the feedback.
I need a help with CEC signal in HDMI , if i am not using what should i do .
can i leave it floating, or should i connect it to ESD diode IC and just pull it up .
Thanks,
Irfan
Irfan
This pin is either NC or can be routed to control a CEC enable FET as shown below.

Thanks
David