Part Number: SN65HVD1781-Q1
Tool/software:
Dear TI experts,
My customer failed EMC CE current test of their product using SN65HVD1781-Q1.
1) Average and peak values are exceeded in measuring CE Current in 80~90MHz bandwidth.
2) Max exceeded value of peak is -6dB, max exceeded value of average is -6dB (did not save measured data)
3) Exceed values are disappeared if RS485 communication is disabled.
4) Customer uses extended cable for RS485, and symtoms are different regarding to the location of cable.
5) Communication setup : 115200 baud rate, 200ms communication period.
Here are my questions;
1) Is there any specific guidelines for EMC CE current test?
2) Could you advice for have more margins to pass the test?
I attach the test results and schematic.
CE-S_Add signal line, Add GND.pdf
CE-S_Add signal line, Remove GND.pdf
Best regards,
Chase