This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS31: SN65LVDS31DG4 and SN65LVDS32D's transmission length when the two are connected

Part Number: SN65LVDS31


Tool/software:

Hi 

SN65LVDS31DG4 and SN65LVDS32D's Single end to LVDS IC (T/RX) architecture, what is the maximum transmission length when the two are connected?

For example:
At 50MHz, what is the maximum length limit/recommendation?
At 100MHz, what is the maximum length limit/recommendation?