This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848YB: DP83848YB IBIS model issue

Part Number: DP83848YB

Tool/software:

In the DP83848YB IBIS model, the Signals RD+/-  and TD+/- are mentioned as NC. How to use this model for SI Analysis?

Following is the section of ibis file

|
|****************************************************************************
[Copyright] Copyright 2010, National Semiconductor, All Rights Reserved
[Component] DP83848YB
[Manufacturer] National Semiconductor Corporation
|
[Package]
| typ min max
R_pkg 0.140 0.127 0.157
L_pkg 3.582nH 3.226nH 4.234nH
C_pkg 0.191pF 0.166p 0.225p
|
[Pin] signal_name model_name R_pin L_pin C_pin
|
1 TX_CLK g24q370 0.15656 4.225n 0.22528p
2 TX_EN g24q370 0.15065 3.8952n 0.22528p
3 TXD_0 g24q370 0.14073 3.5958n 0.19023p
4 TXD_1 g24q370 0.13437 3.4082n 0.17307p
5 TXD_2 g24q370 0.12907 3.2895n 0.16915p
6 TXD_3/SNI_MODE g24q370 0.12691 3.2324n 0.16848p
7 PWR_DOWN/INT g24q370 0.12657 3.2275n 0.16848p
8 TCK g24q370 0.12836 3.2793n 0.16719p
9 TDO g24q370 0.13313 3.3848n 0.17354p
10 TMS g24q370 0.1394 3.5665n 0.18753p
11 TRST# g24q370 0.14814 3.8368n 0.2253p
12 TDI g24q370 0.15432 4.1711n 0.2253p
13 RD- NC 0.15631 4.2018n 0.2255p
14 RD+ NC 0.15131 3.8843n 0.2255p
15 AGND GND 0.15006 3.6114n 0.19977p
16 TD- NC 0.15075 3.441n 0.18844p
17 TD+ NC 0.13739 3.3142n 0.16741p
18 PFBIN1 NC 0.13221 3.244n 0.16625p
19 AGND GND 0.12968 3.2459n 0.16625p
20 RESERVED NC 0.13079 3.2952n 0.16623p
21 RESERVED NC 0.13515 3.4208n 0.17468p
22 AVDD33 POWER 0.14044 3.6002n 0.18892p
23 PFBOUT NC 0.15022 3.8953n 0.22685p
24 RBIAS NC 0.15593 4.2162n 0.22685p
25 25MHz_OUT g24q370 0.15312 4.1446n 0.22587p
26 LED_ACT/COL/AN_EN g24q370 0.14495 3.7933n 0.22587p
27 LED_SPEED/AN1 g24q370 0.13831 3.5685n 0.17558p
28 LED_LINK/AN0 g24q370 0.13314 3.3801n 0.17558p
29 RESET_N g24q370 0.12885 3.2804n 0.16657p
30 MDIO g24q370 0.12704 3.2256n 0.16709p
31 MDC g24q370 0.1273 3.228n 0.16709p
32 IOVDD33 POWER 0.12942 3.2833n 0.168p
33 X2 osc25x2 0.13485 3.415n 0.17683p
34 X1 osc25x1 0.14048 3.607n 0.18272p
35 IOGND GND 0.15068 3.9121n 0.2283p
36 DGND GND 0.15658 4.2288n 0.2283p
37 PFBIN2 NC 0.15676 4.2216n 0.22705p
38 RX_CLK g24q370 0.15083 3.89n 0.22705p
39 RX_DV/MII_MODE g24q370 0.141 3.5979n 0.18895p
40 CRS/CRS_DV/LED_CFG g24q370 0.13461 3.4092n 0.17485p
41 RX_ER/MDIX_EN g24q370 0.12927 3.2882n 0.1673p
42 COL/PHYAD0 g24q370 0.12748 3.2324n 0.16711p
43 RXD_0/PHYAD1 g24q370 0.12747 3.236n 0.16711p
44 RXD_1/PHYAD2 g24q370 0.12931 3.2906n 0.16723p
45 RXD_2/PHYAD3 g24q370 0.13487 3.4154n 0.17475p
46 RXD_3/PHYAD4 g24q370 0.14072 3.6012n 0.18882p
47 IOGND GND 0.15108 3.9084n 0.22706p
48 IOVDD33 POWER 0.15677 4.2336n 0.22706p