Tool/software:
Hi Team,
In the datasheet it is stated that the HSS pin can be programmed to support a 200Hz or 400Hz 10-bit PWM signal via PWM1 or PWM2, and it can be configured to one of the timers to work with the WAKE pin.
Can you please verify if this means that the HSS output pin feeds a 200Hz 10-bit signal towards the WAKE pin?
Can the WAKE pin also be configured to be an input for an external 200Hz PWM signal?
Thanks for a feedback.