This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4E05U06: HDMI output does not work.

Part Number: TPD4E05U06
Other Parts Discussed in Thread: TPD1E05U06, , ESD224

Tool/software:

We designed a board that connects HDMI to HDMI between a PC and a monitor.

We applied the Protection IC, but the HDMI connection is not working.

The TMDS line has 100 ohm impedance.

Currently, HDMI Pin 17 is NC on the circuit, but even if we connect GND, the image does not appear.

The circuit diagram shows that the right side of the HDMI Port is the Monitor side, and the artwork is on the top side of the Monitor side.

Please review.