Part Number: TCA9802
Other Parts Discussed in Thread: ISO1641, TCA9509
Tool/software:
We have processor driving side A of TCA9802 (2.2k pullups).
Then side B of TCA9802 is connected to ISO1641 (side 1) - no other I2C device.
Side 2 of ISO1641 is connected to EEPROM 24LC64.
Processor starts I2C transfer addressing EEPROM, everything goes well until ACK stage: EEPROM pulls SDA down to 0V, ISO1641 pulls down to ist low around 0.5V (side 1). But TCA9802 responds in unstable way, getting into sort of oscillations.
Do you have any suggestions what causing it?
Does TCA9802 (side B) can be interfaced to ISO1641 (side 1)?
Regards
Wojtek

When EPROM device is addressed correctly and responds with ACK but TCA9802 is not responding correctly to this ACK:

When no device is addressed so NACK is correctly generated: