This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] What data rates support which resolutions?

Mastermind 26741 points

Part Number: TDP2004

Tool/software:

Hi Team, 

What data rates for DP and HDMI support which resolutions?

  • Supported resolutions for each data rates are shown below for HDMI and DP:
    HDMI:
    HDMI 1.4 - 4K30 OR 1080p @120Hz
    HDMI 2.0 - 4K60 OR 1440p @ 165Hz
    HDMI 2.1 6Gbps - 4K60
    HDMI 2.1 8Gbps - 5K60 OR 3440x1440 @ 200Hz
    HDMI 2.1 10Gbps - 8K30 OR 4K120
    HDMI 2.1 12Gbps - 8K48 OR 4K120

    DP:
    DP HBR (2.7G) - 1080p @ 120Hz or 1440p @ 60Hz
    DP HBR2 (5.4G) - 3440x1440 @ 60 or 1440p @ 165Hz or 4096 x 2304 @ 60 Hz or 4K60
    DP HBR3 (8.1G) - 3440x1440 @ 120Hz or 4K80 or 5K30
    DP UBR10 (10G)- 3440x1440 a@ 165Hz or 5K60
    DP UBR13.5 (13.5G)- 6K60 or 3440x1440 @200
    DP UBR20 (20G) - 8K60 or 4K165