This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: Transceiver switches to StandBy mode during EMC testing with 8kv

Part Number: TCAN1145-Q1

Tool/software:

Hello,

It was observed during the EMC testing (8kv pulse) that the TCAN1145 transceiver switches to StandBy mode and the communication is not auto recovered without switching the transceiver back to Normal state. During analysis it was found that the transceiver detects under voltage scenario during EMC testing and that is the reason why it moved to fail-safe mode/standby mode.

Is this behavior expected?

TCAN1145 Datasheet states that the "The family comes with high on-chip IEC ESD protection, but if higher levels of system level immunity are desired external TVS diodes can be used." also maximum ESD rating as 8000v.

Could you please share the EMC test reports which was conducted by 3rd party?