Part Number: TUSB320LAI
Other Parts Discussed in Thread: TUSB320
Tool/software:
Hello,
I am currently working on a battery powered product design which features a USB-C UFP. This port is to be handled by the TUSB320LAI, so as to determine the current capability of a plugged source in order to configure a battery charger's C-rate.
Our USB interface supply is currently 3.3V, regulated from Vbus. Hence the TUSB320LAI's Vdd is 3.3V, with startup upon insertion of the source.
I would need clarification on the following statement from the datasheet :
" If a DFP advertises 3 A, system designer must ensure that the VDD of the TUSB320 device is 3.5 V or greater." (§7.2.2 Type-C current mode)
Does this apply only to applications where the TUSB320LAI is embedded in a DFP ? Or does it apply to UFP being presented such 3A-capable DFPs ? I would like to assess whether our UFP with Vdd = 3.3V is going to function properly with a 3A DFP, which will be our main use case.
Best regards,
Martin