Part Number: TCA9416
Other Parts Discussed in Thread: LSF0102, TXB0102
Tool/software:
Is TCA9416 suitable for MDIO level translation from 1.2 to 1.8V? I am a bit unclear if having edge accelerators will help or hurt there. This is on a pretty short and slow bus (1inch long, 1MHz max) with pretty well controlled impedance.
Alternatively what would you suggest we use that is small, and can handle voltages listed?
Ideally the same part could also be used on I2C buses in this design to shift 1.2 to 1.8 as well as 3.3 to 1.8V