Part Number: TCA9803
Other Parts Discussed in Thread: TCA9617B,
Tool/software:
Hi!
I'm looking for enhanced pull up to a system with long cable, but sadly other end has to be unbuffered/ up to spec i2c devices. The cable can be between 400 - 2000pF, i2c speed 100khz and max pull down from spec 3ma.
This buffer should provide very fast rise time, but is there something I'm missing? The datasheet does not show any examples driving over 400pF capacitances? Is there something I should know when using the B side of repeater from controller PCB to drive long CAT6A cable? Noise, overshoot for CC pull up or other concerns? Propagation delay through the buffer + rise time?
System would be something like
Controller MCU -ASide-TCA9803-BSide- RJ45 - 2-6m CAT cable - RJ45 - some sensors. - Chain next cable and some sensors.
Any help on figuring what margins I have for max capacitance/speed or other solutions available to allow high capacitance cable with just the spec 3mA pull up.