This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB3410: X1 / CLKI input voltage

Part Number: TUSB3410

Tool/software:

Dear Team,

Our cusotmer uses a clock oscillator.

What is the absolute maximum ratings of X1/CLKI pin? I think that X1/CLK1 abs is VCC + 0.5.

But, it must not exceed 1.8V as the following.

How should we interpret this?

.

Best Regards,

Sijiro Matsuoka