Other Parts Discussed in Thread: UCC21710
Tool/software:
Hello,
I am encountering an unexpected behavior with my current setup and would appreciate your input.
I’m using the SN65C1167ERGYR differential line receiver to convert a 5V differential PWM signal for interfacing with the UCC21710 gate driver. The differential PWM signal is a 5V, 10kHz pulse applied to pins 1 (A) and 2 (B) of the SN65C1167ERGYR. Please refer to the attached schematic for details.
The issue is that the single-ended output at pin 3 (R) remains stuck at a constant high level (5V), regardless of whether the differential PWM signal is present on the input lines or not.
Could you help me troubleshoot this behavior and point out any possible configuration or implementation errors I might be overlooking?