Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: TCAN1145DMTRQ1

Part Number: TCAN1145-Q1

Tool/software:

Issues:

1. SPI read always return SDO pin as 0xE054 for all registers.

2. SPI write always return SDI pin as 0xE000 for writable registers.

Below are my EBtressos configurations:

Port config:

MISO --> Input to MC, Pull_UP
MOSI --> Output pushpull from MC, ALT3, Idle as low
CS     --> Output pushpull from MC, ALT3, Idle as High
SCLK---> Output pushpull from MC, ALT3, Idle as low

SPI device:

Configured for SPI mode 0.
SPI baud rate as 2Mega.


Note: Used frame if 0xADDR/WData. (as per data sheet)