Part Number: TUSB8041-Q1
Other Parts Discussed in Thread: TUSB319-Q1
Tool/software:
Hi,
There is a Power On Control for Downstream Power Enable which is a pin PWRCTL1/BATEN1 for the Hub Controller IC TUSB8041-Q1. Also, there is an ID pin which is asserted low when the CC pins detect device attachment for CC Controller TUSB319-Q1. I am using both these ICs on my board. So, I wanted to know which pin PWRCTL1/BATEN1 of the Hub or ID of the CC Controller should be connected to the EN pin of Power Switch.
I also want to connect the ALERT pin from the Power switch to the OVERCUR1z pin of USB Hub controller so that it detects overcurrent if any. So, I am not sure if I will have to mandatorily connect PWRCTL1/BATEN1 of the Hub Controller IC TUSB8041-Q1 to the EN pin of Power Switch.
May I know what will happen if I don't connect PWRCTL1/BATEN1 of USB Hub controller?
Regards,
Adithya