Other Parts Discussed in Thread: SN65LV1023A, TLK1501
Hello,
for an industrial application we would like to transmit 2 signals (TTL level, frequency range DC up to 60kHz) via one optical single mode fiber. The latency should be below 20us.
We have used a fast ethernet fiber transceiver before for a standard Ethernet application and we would like to use the same transceiver for the new project.
Do you have Serializer/Deserializer products which can be used for our application? I noticed that most high speed interface products target higher data rates than fast ethernet or even industrial signalling applications.
I identified the SN65LV1023A as a potential candidate for our "low speed" application but I have not found application notes for a fiber transmission (only copper). Other suggestions of SerDes solutions are also welcome, ideally the SerDes could drive the PECL interface of our fiber transceiver.
It would be helpful to get application notes / reference designs for fiber applications.
Thanks in advance, regards
Karsten Schwinne