Part Number: TMDS181
Tool/software:
Hello,
I use the TMDS181 for redriving/retiming an HDMI signal at the front panel of a device.
Unfortunately, the redriver/retimer is not working reliably. When I plug it in with my laptop as a source and a monitor as a sink, sometimes it works great in 4k, sometimes it doesn't work at all.
I read out the I²C registers and noticed 3 registers differ in the IO to the NIO case:
Reg 0B: Bit 4 is off in IO and on in NIO, so the termination changes from 150-300 Ohms (IO) to 75-150 Ohms (NIO)
Reg 15: Bit 7 is on in IO and off in NIO, so the deskew is not finished in NIO
REG 20: Bit 6 is off in IO and on in NIO, so the device goes to standby in the NIO case.
Could you please help me find the root of the instability?
Best regards,
Jonas