Part Number: TUSB321AI
Other Parts Discussed in Thread: TUSB322, TUSB542, TUSB321
Tool/software:
Hello,
We are using TUSB321AIRWBR and TUSB542RWQR.
TUSB is set to UFP mode.
CC1, CC2 are swapped as mentioned in the TUSB542 datasheet (there is TUSB322, but the logic should be the same as TUSB321, right?)
one type-c side:
CC1 => 5V
CC2 => +- 1.8V
DIR => 1.8V => ok
second type-c side:
CC1 => 0V
CC2 => 5V
DIR => 1.8V (should be log. 0?)
It also works differently on different PC ports and cables (we tried a lot of cables and PCs)
On Type-C to Type-C connection with a PC, it doesn't even wor,k while with USB-A to USB-C connection (USB-A is the PC side), USB3 works on one side and USB2 on the other side (mux is not switched).
First, we thought that the USB connector was not assembled correctly, but now, we have are sure that everything is done well.
Is there something we might have missed?
Here are also schematics for the CC controller and the MUX