Part Number: THVD1400V
Other Parts Discussed in Thread: THVD2419, THVD1419, THVD1400, THVD2429
Tool/software:
Hello,
I’m using the THVD1400VDRCR IC in an RS-485 application, where the A and B pins are routed to external terminals for field connections (e.g., to an access controller). The IC is powered with 5 V, and A/B are protected with a bidirectional TVS diode to ground.
I want to better understand the real-world failure conditions for this device.
In one instance during testing, the IC was damaged while the board was powered ON (12V supply).The chip heated up rapidly, and the transceiver became non-functional, with A pin showing a short to GND and system 5V showing a short to ground as well.
So I’m now looking for clarification on:
-
Under what scenarios can the A/B pins cause permanent damage to the IC?
-
For example, if someone accidentally connects 12 V DC or shorts A or B to GND, does the internal protection or the TVS handle that safely?
-
Are there known cases where surge, bus contention, or continuous overvoltage can lead to internal shorts or overheating?
I’m trying to build robust protection into the design and would appreciate guidance on:
-
Worst-case conditions that can cause the transceiver to fail
-
Whether series resistors or isolation are recommended
-
Any application notes or stress test data available for reference