Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: Tying EN to 1.8V

Part Number: PCA9306
Other Parts Discussed in Thread: TCA9406, LSF0002

Tool/software:

Hey team,

Engineer is trying to use PCA9306 as a 1.8V to 3.3V translator for I2C. Issue is, the 3.3V supply will be up before the 1.8V supply. 

Ideally, we would like to isolate the 3.3V supply from the 1.8V supply until EN comes up.

In the PCA9306 "normal setup" (figure 8-1 in the datasheet) we see EN tied to VREF2 which is tied through resistor to VCC2 = 3.3V

Is it possible to instead tie EN to VCC1 = 1.8V such that the TRX is not enabled until 1.8V comes up? Or is it possible to connect VREF1 to 3.3V and VREF2 to 1.8V?

If it is not possible to achieve what we are looking for with PCA9306, is it preferable to use TCA9406 here?

Thanks!

Austin Allen