Part Number: DS125BR800
Tool/software:
Hi,
Using the DS125BR800 for 10Gbps PCIe communication with a differential impedance of 100Ω (50Ω single-ended),
please specify the recommended AC coupling capacitor values for both the Tx and Rx sides of the DS125BR800.
Additionally, due to system constraints,
it is necessary to connect two AC coupling capacitors in series on the Tx side.
• One of the capacitors is located on the module and is fixed at 100nF. What should the value of the other capacitor be?
• I would also like to know whether DC bias is required in the section between the capacitors.