Part Number: TS3DV642
Tool/software:
Hi All,
I have a question about the TS3DV642.
There are two LVDS signals for video.
I think it is possible to input these two LVDS signals into the TS3DV642 and output one of the signals, but is that correct?
One thing to be careful of is that it cannot be used if VCC=1.8V. Is there anything else I should be careful about?
Best Regards,
Ishiwata