Other Parts Discussed in Thread: TUSB2046B
Hi Guys
I am working on a School Class Project and try to build up an 1.1 USB Hub with the IC TUSB2046.
I used the reference design for a Self Powered Hub from TI (Available on Product Site of TUSB2046) without the EEPROM and design my own Schematic (Attachment).
So I tied RESET and EXTMEM to 3.3V, EEDATA to Ground and left EECLK floating.
So my qustion is, do i need the EEPROM with VID and PID or is it possible to run this IC without EEPROM?
I have already build a PCB but it doesn't work and I don't know if the error is the missing EEPROM.
greets
Michael
EDIT:
Problem Solved
Stupid Mistake, forget the transistor and pull ups from 3.3V to DP
IC also runs perfectly without EEPROM, default VID and PID is implemented.