This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2036: Reset pulse width

Part Number: TUSB2036

Tool/software:

Dear Team,

My customer is considering the TUSB2036 application circuit desgin, and  is considering to use a Reset IC to /RESET.
The TUSB2036 datasheet describes as below,

 - /RESET: Generally, a reset with a pulse width between 100 μs and 1 ms is recommended after 3.3-V VCC reaches its 90%.

If the delay time of a Reset IC is longer than 1ms, for exampl 100ms or 200ms, is there any probles with the TUSB2036 operation?

Best Regards,

Koshi Ninomiya