Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2E11: Did TUSB2E11 follow Intel CFP design?

Part Number: TUSB2E11
Other Parts Discussed in Thread: TUSB2E221

Tool/software:

Dear team

It seems our TUSB2E11 didn't follow Intel CFP desigm:

Intel spec:

Vendor

Part number

 Pin number

Package

TI

TUSB2E11(single channel)

15 pin

DSBGA,15 (1.75mm x 1.05mm)

TUSB2E221(dual channel)

25 pin

DSBGA, 25(2mm × 2mm)

20 pin

WQFN ,20(3mm × 3mm)

 

 

Intel

Channel

 Pin number

Package

eUSB2 Repeater

Platform Component Specification (PCS)

single channel

12 pin

CSP (1.18mm x 1.55mm)

12 pin

QFN (1.75mm x 2.2mm)

dual channel

25 pin

CSP (2mm × 2mm)

20 pin

QFN (3mm × 3mm)

Do we have part that follows single port Intel CFP design?

Thank you

Charles