Part Number: TSD36
Tool/software:
Hi team,
Could you let me know the maximum voltage of VBR?
The protected device's maximum input voltage is rated at 70V.
In this case, is Vclamp(max)=67V the parameter I should refer?
I'm not sure how to calculate the surge current, but the application is motor drive, so I believe IEC61800 could be reference.
Best regards,
Kazuki Itoh