Other Parts Discussed in Thread: TUSB2046B
Hi,
I've some trouble using a TUSB2046B on my board. I'm using the circuit shown in the datasheet of the TUSB2046B, figure 13 (self-powered hub, individual-port power management). Actually, I'm working with Windows XP SP3. After connecting the device, Windows searches for drivers and installs the "usbhub.sys" (Should be ok, in my opinion.), but then, another window pops up - "unknown device". The device manager indicates an error "code 41". I've already searched the web and there are a lot of problems using usb devices and this error code, the solution seems to be cleaning the registry, but I'm not sure.
Maybe another one already solved the problem.
Bye,
Christoph