This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2046BVF USB Hub chip



We are using the TUSB2046BVF USB Hub chip in one of our designs. During a review I noticed that the implementation wasn't quite in line with the datasheet terminal function specification. The Hub chip is equipped with a serial interface (EECLK/EEDATA) capable of reading Device ID etc, from an external EEPROM. Since we are not using this feature, the EXTMEM# pin is pulled high (deasserted).

The datasheet state that if EXTMEM# is high, the EECLK terminal is disabled and must be left floating (unconnected). In this design, however, this is not the case. We have erroneourly pulled the EECLK pin high through a 1KOhm resistor. The design is currently undergoing a revision where EECLK will be left floating.

I would, however, very much like to know, if pulling EECLK high will have any side-effects on the functionality of the TUSB2046BVF. We haven't so far observed any malfunction that we would expect to be associated with the USB Hub circuitry