This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1057A-Q1: Inquiry about the maximum current consumption when VCC = VIO = 3.3V

Part Number: TCAN1057A-Q1


Tool/software:

Hello.

I have checked that the TCAN1057 IC enters protection mode when VCC is below 3.5V.

However, could you please let me know the maximum ICC of the TCAN1057 IC under the following conditions?

  • IC: TCAN1057AVDRBRQ1
  • S (pin no. 8): GND
  • VCC (pin no. 3): 3.3V
  • VIO (pin no. 5): 3.3V

Regards,

WG Jo