Part Number: DP83867IS
Tool/software:
Hi,
1. In the case of a two-power supply configuration, I think power sequencing is not necessary. Is this correct?
2. When VDD1P0 (VCC_1.0V) is applied, there is a voltage shift of about 250mV before VDDIO (VCC_1.8V) is turned on. Is this a problem?
If VDD1P0 is not applied, there is no voltage shift, so this is probably a leakage voltage from inside the IC.
3. There is a voltage shift of 650mV from the start of the PL_3.3V power supply, another power supply on the board, until VDDIO (VCC_1.8V) rises. Will this have any effect on ETH-PHY?
CH1: VCC5V
CH2: PL_3.3V
CH3: VCC_1.8V (VDDIO power supply)
CH4: VCC_2.5V (VDDA2P5 power supply) At the same time, VCC_1.0V (VDD1P0 power supply starts up)
Best regards,
Hiroshi